| Bryant Electric Announces LED Nightlight Devices |
| Wednesday, January 20, 2016 |
| |
Bryant Electric Announces LED Nightlight Devices
Bryant Electric is excited to announce its new LED Nightlight Devices.
This family of products combines the function of a wiring device with the convenience of a nightlight.
Ideal for use in both commercial and residential applications, these devices can be used as an alternative to
plug-in nightlights. Developed for permanent installation, photocells automatically turn the nightlight on and
off depending on the amount of ambient light present in the space.
Bryant’s LED Nightlight Devices are available in three options:
- Nightlight Decorator Switches feature an impact-resistant
rocker and base, and provide a 0.5-lumen nightlight
- Nightlight Receptacles offers a tamper-resident duplex
receptacle that complies with NEC Article 406.12, along
with two LED nightlight sources that provide 0.5 lumens of
light
- The Nightlight Only option is a full-face lens with maximum
illumination, providing 1.5 lumens
“Not only do Bryant’s new LED Nightlight Devices provide safe light
when ambient light isn’t available, but they’re also an energyefficient
option,” says Vic Flagello, director of residential marketing
for Bryant Electric. “The devices only consume between 0.5 and 1
watt of electricity.”
These devices also ensure that outlets aren’t occupied by plug-in
nightlights, keeping them available for other devices that might
need to be plugged in.
For more information about Bryant Nightlight Devices, to receive a copy of the Nightlight Devices Literature,
or any of their other industrial, commercial, or residential products, visit the Bryant website at
www.bryant-electric.com or contact Bryant customer service at 800-323-2792.
|